(0)| 10/11/2024 10:48 AM | |
|
Joined: 8/3/2021 Last visit: 10/3/2025 Posts: 133 Rating:
|
I write here all history of changes cos I don't know what could be a source of my problems.... I have had installed TIA Portal V13 + V14 + V16 including STEP7 / WinCC ADV / PLCSIM / STARTER. Everything worked ok including projects upgrade V14 to V16. I've made some testing with TIA Portal V17 and V18 trials. But I finally uninstalled them. Everything (V13+V14+V16) worked ok still. Our company has made decision to move to V19. So I've made these steps: 1. I unistalled some Siemens components that looked like leftovers of V17+V18 (TIA Administrator V17/V18, and others) via Windows Control panel. 2. I installed TIA Portal V19 including STEP7 / WinCC Comf-Adv / STARTER. RESULT: - TIA Portal V19 works ok - TIA Portal V16 works ok BUT !!!: - TIA Portal V14 crashes when closing it - TIA Portal V16 isn't able to open (=upgrade) some of V14 projects So far I have tried to: - Reinstall V14 (full uninstall + full new install) - it hasn't helped. Now it's a question if the problem of TIA project V14->16 failed upgrade is related to executed changes (removing V17/18 leftovers; V19 install), TIA V14 crash (probably some damaged ?). OR failed upgrade is related to V14 projects ONLY (they are incompatible ? missing libraries ? damaged?). Upgrade failed report included... AttachmentConversionLog_14.0.1.0_to_16.0.0.0.xml.docx.zip (193 Downloads) |
|
TIA Portal V13/14/16 |
|
| 10/14/2024 6:14 AM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Hi, in newer TIA versions, some HMI are not supported anymore. Check this FAQ: When upgrading your TIA Portal project to V15 or higher, why do you get this error message: "The device [XY] is not supported in this version."?If the complete type is not supported anymore, you have to change the complete HMI. If just the OS version is not supported anymore, you can change the OS version of the HMI before the project upgrade. But its possible that it will require an upgrade to V15/v15.1 first, to be able to choose the OS version supported by V16. regards sancruz |
|
Feedback appreciated, please rate |
|
Follow us on