(0)| 10/27/2024 8:49 AM | |
|
Posts: 1 Rating:
|
I am using Micromaster 440 in my machine. Details of drives are as follows, All Drives are Three Phase Drives. 100KW - 2 Drives 40 KW - 4 Drives 18.5KW - 4 Drives 5.5 KW - 4 Drives Drives of 100KW & 40KW are running properly and they are not tripping. But Drives of 18.5 KW & 5.5 KW are frequently tripping and shows error of F0002 & F0003 (Approximately 15 times in 24Hrs) . These drive trips randomly and sometime error is F0002 & sometime it shows F0003. I have checked voltage and they are very stable. can any one help in this matter to Solve the problem. Power supply is 380V P0210 = 400V In all Drives. I have attached tripping data for reference with date and time. AttachmentDrive Tripping Data.pdf (869 Downloads) |
Follow us on