(1)| 11/14/2024 9:04 PM | |
|
Joined: 5/6/2022 Last visit: 1/21/2026 Posts: 589 Rating:
|
Hi John0196, What I can think of, in case it could help you to check that you don't have cloud connection is the following: 1. Check the Configuration: Ensure that your LOGO! device is not configured to connect to any cloud services. This can be verified by checking the settings in LOGO!Soft Comfort. Specifically, you should not have any cloud connection settings configured under Tools -> Transfer -> Cloud Connection Settings. 2. Network Monitoring: Monitor the network traffic from your LOGO! device to ensure that it is not communicating with any external cloud services. This can be done using network monitoring tools to capture and analyze the traffic. 3. Disable Cloud Features: If your LOGO! device has any cloud-related features enabled, disable them. This includes any settings related to AWS, Azure, Alibaba, or general MQTT configurations. 4. Documentation: Document the steps you have taken to ensure that no cloud connections are being used. This documentation can include screenshots of the configuration settings, logs from network monitoring, and any other relevant information. By following these steps, you can demonstrate that your LOGO! device is not using any cloud connections. I hope this can be of help or support to you. Best regards |
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
| 11/14/2024 10:23 PM | |
|
Joined: 4/1/2024 Last visit: 10/23/2025 Posts: 19 Rating:
|
Yes, this is what I was looking for. Appreciated! |
Follow us on