11/19/2024 10:24 AM | |
Joined: 10/13/2022 Last visit: 8/28/2025 Posts: 2 Rating:
|
Hello, I have problem with this automatic login. With this property checked my application starts without login display, but the logged user is not available in IO field (tag: @UserName), LogOff function triggered by Logout button doesn't work and Login button is not active even if logged user has proper rights. (see att.1) If automatic login is unchecked, first of course I have to log in, but then everything works as it should (att 2). Additionally only in this mode missig license message appears from time to time (att 4). Could it be the problem with the proper license? I'm using only Trial version of Wincc Unified v.17 (att. 3) since I haven't decided yet which HMI platform choose for my future WEB application. Can someone explain how to solve this issue? Regards, Krzysztof ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 11/19/2024 11:48:14New subject after splitting |
|
Follow us on