11/27/2024 8:27 AM | |
Joined: 2/17/2020 Last visit: 9/16/2025 Posts: 1251 Rating:
|
Hi, I believe that the "Allen Bradley - Ethernet IP" communication channel in WinCC V8 does not support redundant Allen Bradley PLCs. The Allen Bradley controllers supported by the channel, as well as the configurable parameters are listed here: WinCC V8 communication > Allen Bradley - Ethernet IP If you have this requirement, there may be solutions based on OPC instead. |
A rating will be well appreciated. |
|
This contribution was helpful to
1 thankful Users |
Follow us on