1/9/2025 6:37 PM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
From what you say it seems a strange behavior, since it seems strange that the logs do not show any kind of error and that the license in the ALM that you indicate is marked as not in use. In this case, at first it could seem to me that There is maybe a Windows Error or Internal service error. Or maybe a certificate problem. To start with I would recommend you to renew the OPC UA Certificates on the system following this FAQ: "Create new CA certificate for OPC UA in WinCC SCADA" Please also make sure that the OPC UA Server is activated in the start-up list of the runtime settings. Best regards!
|
If this Information really helps, you could use the Rate function |
|
Follow us on