1/20/2025 7:12 PM | |
Joined: 9/17/2024 Last visit: 2/9/2025 Posts: 8 Rating:
|
Hi all engineers! I don’t understand how to connect ET200SP CPU 1510 to PCS7 project as DP slave. I used PCS7 v.9.1. My project based on the CPU S7 410-5H: 6ES7 410-5HX08-0AB0. At the one of the PN ports I have PN network. IE/PB LINK HA gateway 6GK1 411-5BB00 is connected to this network. Among of other DP slaves in the DP network of the IE/PB LINK I’m trying to integrate ET200SP CPU 1510SP-1 PN 6ES7 510-1DJ01-0AB0 as DP slave by GSD file. I found GSD file by the link: https://support.industry.siemens.com/cs/de/en/view/113652 I used GSD file forStation type:ET 200SP CPU + CM DP module as my situation is Order no.:6ES7 510-1D*-0AB0 +6ES7 545-5DA00-0AB0 GSD file was integrated to PCS7 project successfully. I set I and Q area for DP slave. After this, I created project in the TIA Portal v16 for ET200SP CPU 1510SP-1 PN and CM DP module. For the CM DP module I set the settings:
DP master for CM DP module remains not assigned. After all this I downloaded PCS7 and TIA projects to CPUs. In the PCS7 project In the Hardware in online mode ET200SP CPU is not available for CPU S7 410 5H as DP slave. But in the application “NCM S7 Diagnostic” ET200SP CPU is available as node with his private PB address in the section “Nodes”, but in the section “DP master” ET200SP CPU is not available as DP salve and has marked as with bad configuration. In the TIA project in online diagnostic I see Error message: “IO Device failure” Event ID: 16# 02:39CB So where I’m wrong, what’s settings not made by me? Is it enough to configure ET200SP CPU for connect to DP master of other project (S7 410-5H and IE/PB Link in PCS7)? Should I set DP master for CM DP module or it’s could be “not assigned”? Should I set diagnostical address for CM DP module same as in the PCS7 project for DP slave, also about Network Id? Or I must to create in the TIA project additional IE/PB link and CPU S7 410-5H with same settings? |
Last edited by: 9Icypaman at: 01/20/2025 19:17:12Last edited by: 9Icypaman at: 01/20/2025 19:18:45 |
|
1/21/2025 3:27 PM | |
Joined: 10/16/2020 Last visit: 9/8/2025 Posts: 146 Rating:
|
Hi! These links may help you with some of your questions:
BR |
If this information has been helpful to you, please don't forget to rate it. |
|
1/22/2025 10:48 AM | |
Joined: 9/17/2024 Last visit: 2/9/2025 Posts: 8 Rating:
|
thanks for articles, but why in the example project of 2nd link it's possible only to add input data. Also this way just allow to connect by DX mode with DP slaves which are part of one PCS project, it's not allow to select other DP address. Also IE/PB Link as DP master don't allow to create DX/MS exchange in PCS7 project. So in TIA portal ET200SP CPU just allow to select MS mode. And should I to create in TIA project same IE/PB coupler for that's ET200SP CPU know who is DP master? |
Last edited by: 9Icypaman at: 01/22/2025 10:53:40 |
|
1/22/2025 10:54 AM | |
Joined: 9/17/2024 Last visit: 2/9/2025 Posts: 8 Rating:
|
And how I can to connect S7 410-5H with IE/PB link in PB subnetwork with ET200SP CPU as DP slave by GET/PUT blocks? |
Follow us on