1/15/2025 7:16 AM | |
Joined: 9/30/2016 Last visit: 8/13/2025 Posts: 946 Rating:
|
Please also see the attached screenshots in this topic and my own first answer. We have a machine where the PLC parts of an alarm have been deleted. However the alarm has not been deleted from the WinCC part of the SW. Unfortunately this means that the machine has 2 constant lines (a message and a warning) in the alarm list with the no longer relevant alarm (see pic 3). From the deleted PLC logic I have decided that it was DB1200.DBX8.5 (coming from either M101.4 or M500.0) that was generating the alarm but I checked with a watchlist that neither of these signals was true (see pic 1). On displayF1_1_Drift.pdl I can see that the tag in WinCC is -FA1_V2_G1_MA1.STATUS (see 4.jpg) so I searched in the Tag Manager for FA1_V2_G1_MA1 (see pic 4,5,6,7 & 8). I also searched in the Alarm Logging for the tag (see pic 9, 10, 11 & 12) I also tried searching for "MO#" and "Udsugning" in most of the groups but with no success. AttachmentKALFA1.zip (109 Downloads) |
Follow us on