1/20/2025 8:53 AM | |
Joined: 5/6/2022 Last visit: 9/15/2025 Posts: 589 Rating:
|
Hi gm2410, In the end, if you make the changes in a V7.5 SP2 software and then you intend to work with a WinCC with V7.5 version, it will not be possible because having modified the project with a higher version you will have made a migration of the project and therefore, you will not be able to work with it with a lower version. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on