(1)| 3/10/2025 6:59 PM | |
|
Joined: 3/14/2008 Last visit: 1/23/2026 Posts: 2233 Rating:
|
Hi, It really depends which changes you need to download. In most cases, an OS download change is sufficiënt. But sometimes the amount of changes are so big, they cannot be downloaded with a change. This is checked upfront before download of the server(s). Some changes need a full OS download. In a non-redundant system, it means the operator looses visualization. In redundant OS server system, you are able to download each server fully one after another so the operator won't loose visualization. Changes that need a full download:
Take a look at the PCS 7 Compendium Part A chapter 11. There is described what it means to download changes or a full download. |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 3/11/2025 5:57 AM | |
|
Joined: 5/21/2013 Last visit: 1/18/2026 Posts: 30 Rating:
|
Thanks, Oreca However, my question was related to OS client download not OS server download |
| 3/11/2025 6:04 AM | |
|
Joined: 3/14/2008 Last visit: 1/23/2026 Posts: 2233 Rating:
|
Hi VeeKy, Oh I'm sorry, I misread your post. OS client is only to be downloaded if you made changes in the OS client project like for example:
A normal procedure looks like this:
You won't need to download the OS client in this case. |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 3/11/2025 1:04 PM | |
|
Joined: 5/21/2013 Last visit: 1/18/2026 Posts: 30 Rating:
|
Thank you |
Follow us on