(0)| 4/5/2023 2:59 PM | |
|
Joined: 8/12/2021 Last visit: 1/20/2026 Posts: 351 Rating:
|
Hi Kaleelmohamed! I suggest you to check the parameters of the connection setup according to the manual. It is possible that the version of the instruction is not correct. On the other hand the error code may be being overwritten. I advise you to use an error logic (save status in an auxiliary variable when the error is triggered) to see if another code appears.
|
|
If this Information really helps, you could use the Rate function |
|
| 4/1/2025 6:19 AM | |
|
Joined: 3/6/2025 Last visit: 7/15/2025 Posts: 4 Rating:
|
I have the same problem any help for solution? Do you even solve the problem? |
| 11/25/2025 10:33 AM | |
|
Joined: 6/28/2016 Last visit: 11/25/2025 Posts: 19 Rating:
|
You need to manually enter the ID in the DB from the mb_client function. |
Follow us on