(0)| 5/9/2025 8:17 AM | |
|
Joined: 9/16/2024 Last visit: 5/9/2025 Posts: 1 Rating:
|
Hello, How can I import a file with SIMATIC SD format to TIA Portal via Openness? I have safety FCs in KOP and want to export and import them with TIA Openness. The export function works, but I do not know how the import function works. In the documentation from Siemens is only an example for the export function: Representation of LAD program code in SIMATIC SD format (S7-1200, S7-1500) • Creating and managing blocks • Reader • TIA Portal Information System Can someone give me an example for the import function? Do I need to import the file with the ending ".s7dcl" and the function ImportFromDocuments? When I export the FC, then I have two files (.s7dcl and .s7res) and I do not know, if I have to import the .s7res file, too... Kind regards, ------------------------------------------------------------------------------------------ |
Last edited by: mau_reis at: 05/09/2025 08:19:13Last edited by: Moderator_Lan at: 05/09/2025 08:28:32New subject after splitting |
|
| 5/19/2025 10:33 PM | |
|
Joined: 9/18/2024 Last visit: 7/4/2025 Posts: 2 Rating:
|
Exporting program block as document • TIA Portal Openness: API for automation of engineering workflows • Reader • TIA Portal Information System |
This contribution was helpful to
|
|
| 6/18/2025 12:38 PM | |
|
Joined: 12/4/2024 Last visit: 8/26/2025 Posts: 5 Rating:
|
sample code [attached] Attachment0618_sample code.txt (116 Downloads) |
Last edited by: Moderator_Lan at: 06/18/2025 13:59:47Code attached for better legibility |
|
Follow us on