(0)| 7/14/2025 1:42 PM | |
|
Joined: 8/3/2009 Last visit: 1/20/2026 Posts: 16653 Rating:
|
Hello xoptopus WinCC V8.1 should be compatible with MS Server 2022 (like listed in compatibility list) does the Webconfigurator runs without problems? Check after the run and a PC restart if the IIS Website with Webnavigator is running in IIS Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
| 7/16/2025 4:46 AM | |
|
Joined: 7/11/2025 Last visit: 7/17/2025 Posts: 2 Rating:
|
Hi Murof, I seem to have resolved the IIS issues. However, now the webnavigator won't connect. I'm getting the "failed to load https://XXX.XXX.XXX.XXX:4430/mainmenu.pd_" error. I don't understand. I'm doing everything according to Siemens' own documentation, but the system isn't working on Server 2022. I installed Server 2019 and it didn't work on that either. I wonder if Siemens claims these systems are compatible without testing them. Everything I've done is according to the original Siemens documentation. I've made all the settings as instructed, but I still can't get the webnavigator client to work. |
| 7/18/2025 12:33 PM | |
|
Joined: 8/3/2009 Last visit: 1/20/2026 Posts: 16653 Rating:
|
Hello xoptopus do you have opened already a Service request at Siemens Support? Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
| 12/3/2025 9:12 PM | |
|
Joined: 5/12/2025 Last visit: 1/19/2026 Posts: 2 Rating:
|
Experiencing the same issue, anyone with a Solution? |
| 12/4/2025 10:56 AM | |
|
Joined: 5/9/2018 Last visit: 1/16/2026 Posts: 38 Rating:
|
If you are experiencing the error “failed to load https://XXX.XXX.XXX.XXX:4430/XXX.pd_”: |
Last edited by: Moderator_Lan at: 12/04/2025 12:13:37invalid link removed |
|
Follow us on