7/26/2025 7:19 AM | |
Joined: 5/26/2011 Last visit: 9/16/2025 Posts: 483 Rating:
|
Good day. There is a PCS7 v8.0 SP2 system already working with all single AS connected to a server pair. They only use normal onboard LAN card on ES and OS servers for plant bus (no CP1613). Now we want to add their first redundant S7-410H to this system. I read many thread that for redundant S7-400H to communicate to ES and Server you need CP1613 and Redconnect license, but most discussion I see are old ones. I want to confirm if this is still needed for PCS7 v8.0 SP2 system? Because I also seem to find a section in PCS v8.1 manual that appears to say plant bus can accommodate fault-tolerant S7400H without CP1613? But on the next paragraph it appears to say if using S7-410H CP1613 + redconnect is always needed.. I also find a thread in which someone said he managed to make it work in PCS7v8.0 SP1 (PCS7 with F/FH Systems:PCS 7 V8.0 Update 1 vs PCS 7 V8.0 SP1 - Siemens SiePortal). Please clarify experts. Thank you so much. |
Last edited by: G_R_E_Y_31 at: 07/27/2025 23:21:41 |
|
7/27/2025 8:18 AM | |
Joined: 12/22/2021 Last visit: 9/16/2025 Posts: 60 Rating:
|
Hello G_R_E_Y_31
|
Follow us on