7/10/2009 11:10 AM | |
Joined: 3/18/2009 Last visit: 12/6/2024 Posts: 306 Rating:
|
This is already answeredhere. |
7/10/2009 11:17 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi I can advice you the getting starteds of PCS7 so you get a very good impression, how to work with PCS 7 efficiently. getting started part 1 http://support.automation.siemens.com/WW/view/en/36191439 getting started part 2 http://support.automation.siemens.com/WW/view/en/36191460 In part 1 is a step by step discribtion of the Hardware configuration of the as and the os. additional questions are wellcome regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
This contribution was helpful to
1 thankful Users |
7/15/2009 6:00 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi Sorry missunderstanding. Ok you use a DP/PA Coupler and a PA loop.From the PA loop you get Pressure,Temperature.Flow,Level,Vibartion by transmitters. Right? here themanuel of the DP/PA(Profibus), that should help. http://support.automation.siemens.com/WW/view/en/1142696 To install the GSD-File open in the SIMATIC Manager and the HW-Confic-Editor. Click in the menübar at "Options" > "Install GSD File" How to configure it, i can not tell you, i do not work with pa, sorry. regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
Follow us on