5/13/2009 8:19 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, For me it's not so clear what you mean with "other software". Anyway about migration look at http://support.automation.siemens.com/WW/view/en/24450444 Regards Hristo Mihalev |
5/13/2009 8:39 AM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi salman,
what do you really means: - integrated in Simatic or just having access to PCS7 database? - installed on same station or installed on different station wirh data exchange? It will better have a list of that "external" SW to give you an hexaustive answer. Anyway, just for starting: PCS7 v6 was working on Win 2K and MSQL 2000 SP3, PCS7 v7 it works over Win Xp SP2 with MSQL2005. Check compatibility between "not Siemens application" and new platform at first. Then check the manual UMENCHOgave to you. Regards |
5/13/2009 2:45 PM | |
Posts: 17 Rating:
|
what is the process to convert the pcs7v6.0 project to pcs7 v7 .0 |
5/13/2009 4:10 PM | |
Posts: 2661 Rating:
|
Hi salman92, The procedure is described in the link posted by UMENCHO! Regards |
5/15/2009 6:47 AM | |
Posts: 17 Rating:
|
Ihave one server and client with no engineering station and pcsV6.0 is used so i have toupgrade the system with siemens PCS7 V7.0 |
5/16/2009 7:53 AM | |
Posts: 2661 Rating:
|
Hi salman92, Sorry but I am totally confused now! Do you mean you have no ES (Engineering Station)? Without ES no migration is possible... Regards |
Follow us on