(0)| 8/31/2009 11:45 AM | |
|
Posts: 101 Rating:
|
Hi, find below the code program that i thought it might be of help for you. ***in main*** ************************************************************************************************************** ORGANIZATION_BLOCK MAIN:OB1 TITLE=PROGRAM COMMENTS BEGIN --------------------------------------- Network 1 // Network Title // Network Comment, the @ sign should be written at the end of every sent message. ------------------------------------------ LD SM0.1 MOVB 16#09, SMB30 MOVB 16#B0, SMB87 MOVB '@', SMB89 MOVW +5, SMW90 MOVB 100, SMB94 ATCH INT0, 23 ATCH INT2, 9 ENI RCV VB100, 0 ****************************************************** ***in INT0*** Network 1 // Network Title LDB= SMB86, 16#20 LPS MOVB 255, SMB34 ATCH INT1, 10 AENO S M0.0, 1 LRD CRETI LPP NOT RCV VB100, 0 ****************************************************** ***in INT1*** Network 1 LD M0.0 LPS DTCH 10 AENO = Q1.0 LRD XMT VB100, 0 AENO R M0.0, 1 LPP CRETI ****************************************************** ***in INT2*** Network 1 LD SM0.0 RCV VB100, 0 END_INTERRUPT_BLOCK ************************************************************************************************************ All you need to do is to enable STL coding on your microwin instead of LAD. cut and past the above code and compile and download. NOTE: this code can also be seen as LAD, go to view, then click on LAD, then the code will be converted to LAD. The above code is only for freeport 0 if you are using s7200 -CPU 224XP. Actually, all you need to do is to send your data in the PCs' terminal in the order you want. In the PLC side, the data is received in VB100; VB100 is only the starting index to a virtual table(TBL) in which all data that you send will be saved. the code allows you to send up to a maximum of 100 bytes in one dump, this 100 can be changed if you want to; just move the 20 to SMB94. however don't forget the terminater that you should send at the end of your message in the PC's terminal, in the code i have made it the @ sign. If you don't send the terminator char, then the PLC's free port will not accept the message. If you want to check the data received in the PLC, you have two options to achieve that: - Either by clicking on the Status Chart and from there you input vb100 and then click on theglasses button to see what data actually received. - Or by checking that through the code, and here is the code: ***************************************************** Let say upon receving the following string: "are you awake?@", the PLC should reply with yes, coded as "y". this can be achieved as follows before the end of main: ***************************************************** LDS= "are you awake?@", VB100 MOVB '1', VB200 AENO MOVB 'y', VB201 *******************end of check******************* The reason i moved a dummy char, '1', to VB200 is that it will not be seen at the PC side as you receive the reply message 'y', because it will be eaten as it specifies the length of the string. Let be more specific here, this is because of the following: "The Format of ASCII Constant STRING Data Type: A string is a sequence of characters, with each character being stored as a byte. The first byte of the string defines the length of the string, which is the number of characters. If the constant string is entered directly in the program editor or data block, then the string must begin and end with double quote characters ("string constant"). The memory map below shows the format of a STRING data type. The string can have a length of 0 to 254 characters. The maximum length for a string is 255 bytes (254 characters plus the length byte). " The above code can be seen in LAD if you click on view-LAD. |
Follow us on