9/28/2009 11:35 PM | |
Posts: 2661 Rating:
|
Can you explain? Did you install from the supplied CD? Which WinCC version? See if following are useful: How should you proceed if installation of the Microsoft SQL server fails? Why does the SQL server 2000 SP3 not appear as present during the installation of WinCC V6.0 SP3, even though it is installed? Regards |
9/29/2009 8:34 AM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi control & automation engineer, in PCS7 v7.1 all installation is automatically, but with previuos version you have to perfom some patch installation before proceeding with SQL & PCS7 installation. If you are not installing v7.1 remember to install all patch you need from WinCCTool Set DVD. Maybe installing SP from there can fix your problem. If not, can you give us more info as well as Phantom75like your PC installation and procedure you followinf to install PCS7. Regards |
Follow us on