10/7/2009 10:50 PM | |
Posts: 2661 Rating:
|
Hi echorafo,You need an OpenPCS 7 license, the software is included with PCS7. You canconfigure OpenPCS7 station on OS client, single station or CAS but not on OS server. See possible system configurations in the following manual: SIMATIC PCS 7 process control system OpenPCS 7 Also look at the block diagram in the following link for example of the migration process: PCS 7/OPEN OS V7.1 – Sales and Delivery Release Regards |
Last edited by: Phantom75 at: 10/7/2009 10:59 PMLast edited by: Phantom75 at: 10/7/2009 10:51 PM |
|
10/9/2009 9:14 AM | |||
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi echorafo, i'm a lil confused
PCS7 is not just a SCADA but a complete system where Supervisory comes from plc development. I'm not sure you can program PLC Modicom with PCS7 library. There are special reason you want use PCS7 instead WinCC? Here a previuos post, maybe can help you
Regards |
||
Follow us on