10/15/2009 12:03 PM | |
Joined: 5/31/2007 Last visit: 6/4/2025 Posts: 90 Rating:
|
I installed WinCC K7.0.1.0 in my notebook. When I edit PCS7 project, Ieditmy .pdlfilesby WinCCExplorer Graphics Designer, but Ifind I can't see and selectcolors intheObject Properties of Colors, Anyone can tell me what's the matter?Anything I should watch out?? One file attachment. AttachmentColor_Sel_Trouble.zip (108 Downloads) |
10/15/2009 2:35 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi If i understood you rigth, youcopied the onlythe .pdl and not the hole project. The color, you can not see, is a project setting, not a setting of the picture. You have to create the same colors at the same color-number of the orginal project, than you can see the right color. That means too, you can define other colors the that color-number on your notebook, but you see the rigth color in the orginal project. regards and good luck cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
Follow us on