10/23/2009 9:57 AM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi Delphoe , |
This contribution was helpful to
1 thankful Users |
10/23/2009 11:16 AM | |
Posts: 120 Rating:
|
HI, CBo Here I create 2 project. the first project is a multi station project with Server-CLient OS and It will locate on the computer 1. The second project is a sigle station project with Client OS and will locate on the computer 2. Now what should I do if I want to download the database of OS Server from computer 1 in order to run on computer 2 with the OS Client. I still can't figure out how to carry out this matter. Please help me. Thanks a lots. Regards. AttachmentDesktop.zip (118 Downloads) |
Last edited by: Delphoe at: 10/23/2009 11:17 AM |
|
10/23/2009 11:22 AM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi Delphoe , here a link How do you create a SIMATIC PCS 7 V6.0 SP3 project with S7-400 station, pair of redundant servers and client? i hope can help you Regards |
Follow us on