12/16/2009 12:39 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi guys, When installing pcs7.1 sp1, I encountered problems with installing sql server. I can't remember if it was okay afterwards but the installation of pcs7 was completed. Now something worries me, Before installing pcs7, I had the following siemens software installed: Step7 5.4 HF4 and Wincc flexible 2008 build v1.3. Wincc flexible could be the problem when trying to install sql server. I didn't noticed any errors saying that sql won't function, but the question is if I can uninstall Wincc flexible + SQL server and then install SQL server and Wincc 7.0 from the PCS7 cd? I can't afford the laptop to be formatted and the image file is created after installing Step7+wincc flexible. Thx! |
If I could help you, you can use the RATE button. Thank you. |
|
12/16/2009 2:27 PM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi Sandor-CRX, as well you said WinCCFlex MSQL and PCS7 MSQL are quiete different and not compatible between them. PCS7 and WinCCFlex has not to be installed on same disk partition. About PCS7 v7.1 installation more detailed info are in "PCS7 Readme" manual & "PCS 7 - PC Configuration and Authorization" manual installed with PCS7. I suggest to you to save license and reformat PC, Hope can help Regards |
Follow us on