(0)| 11/30/2009 5:48 AM | |
|
Posts: 107 Rating:
|
Hi, Does any one knows about SIEMENS product for power supply with spec : INPUT 220VAC OUTPUT : +15Vdc 0 -15Vdc CAPACITY : 5A or 10A regards, indra |
| 11/30/2009 6:30 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello indra, Did you mean 6EP1353-0AA00
Best regards, Hristo Mihalev |
| 11/30/2009 6:20 PM | |
|
Joined: 5/28/2008 Last visit: 1/21/2026 Posts: 4522 Rating:
|
Dear isurya, First of every thing, please look here in the following link, go to Sitop catalog: Catalog KT 10.1, SITOP,and download the Sitop catalog 2009 and you will found in it theall Sitoppower supplies: https://www.automation.siemens.com/infocenter/order_form.aspx?HTTPS=REDIR&tab=1&nodekey=&lang=en Siemens offers different power supplies for 15VDC; 15VDC; MLFB: 6EP1352-1SH02. If you connected more than one power supply in parrallel in order to have higher current, it will work. But I recommend if you will do it to design the protection circuit very well or you can make grouping in the load and make common ground for the all power supplies.
The duel power supply 15V has two outputs: it has in the output section the following terminals: +15V 0V of first group & +15V +15V 0V of second group So you can have two deffernt 15 VDC outputs or you canmake jumber between 0VDC of 1st group with+ 15VDC of 2nd group and then you have + 15V; 0V; - 15V like the following: 1st group: +15V .......................... +15V 1st group: 0Vjumpered 2nd group: +15Vjumpered 2nd group: +15V .......................... 0V 2nd group: 0V .......................... -15V See the manual here: SITOP power 2x15V/2x3.5A Hope this helps, |
Last edited by: Ayman Elotaify at: 11/30/2009 6:29 PMcorrection of the link Ayman Elotaify |
|
This contribution was helpful to
|
|
| 12/7/2009 2:52 PM | |
|
Posts: 4 Rating:
|
My opinion is that you can use power supply from another manufacturer with no problems. Many times you save 50% of cost price. |
Follow us on