1/5/2010 9:02 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello Pedro Pablo; If what you are looking for is programming information and code examples for the S7-200, using Microwin, here are the 2 best ways to start: - the S7-200 System manual contains the Microwin instruction set, along with programming concepts for the S7-200 family: http://support.automation.siemens.com/WW/view/en/1109582 - the S7-200 Tips and Tricks is a collection of applications that are proposed by Siemens as a guide for programmers; they contain downloadable code that you can use as a basis for yourprogram: https://www.automation.siemens.com/microset/html_76/support/tipps/index.htm?HTTPS=REDIR Once you have a handle on Microwin, the online help from WinCC Flexible can guide you on connections to the S7-200 PLC, assignment of PLC datatypes and addresses, and various graphic objects you can use to animate the data from the PLC. Hope this helps, Daniel Chartier |
Follow us on