(0)| 1/15/2010 8:19 PM | |
|
Joined: 6/4/2008 Last visit: 11/25/2025 Posts: 1521 Rating:
|
Hi, I hope I can try and shed some light on this, I didn't commission this project, so I'm not 100% how it is done. I have attached a project where the infeed signal from the "SINAMICS_S120_CU320_2" Control Unit is transmitted using the IF words over profibus to the "CAL_AUX" Control Unit (See function diagrams.2460 and 2470) Enjoy!! AttachmentNew.zip (351 Downloads) |
Follow us on