1/14/2010 3:23 PM | |
Joined: 3/14/2008 Last visit: 9/4/2025 Posts: 2216 Rating:
|
Hello guys, I'm engineering the software for a chemical plant. It used to run with PCS7 4.0 but software is gone. I have a CFC print out (not complete, but enough)and I'm rebuilding the software with the help of CFC (never programmed a plant before). For example: I have build two PID controllers which are working in cascade with the PCS7 V71 library. I tryed to reuse the same blocks that are on the CFC printout. I never checked out the AP V71 library, untill today. Now I want your advice on whether to continu on using the PCS7 V71 library or change it using only AP V71 blocks. I saw that the AP library has more and even better blocks. I think that AP V71 is an upgradedlibrary of PCS7 V71. In AP libr. are also driver blocks, PID blocks etc.etc. Which blocks do I need to use? from AP of PCS7 library? I think it is not possible to use blocks both from PCS7 and AP library, but I don't want it either. I saw that the faceplates are much better( look better) than the ones from PCS7 library. I'm not very far with the software, but what do you guys say about this matter. Is switching to AP a far better option? Thank you, Regard, Sandor |
Last edited by: Sandor-CRX at: 1/14/2010 3:34 PMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on