2/7/2010 10:32 PM | |
Posts: 88 Rating:
|
Hi Yer, How to check the AS RT PO License on the CPU? T41 |
2/8/2010 3:43 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi T41, may this FAQ helps you: http://support.automation.siemens.com/WW/view/en/38855207 Regards Cumu |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
2/12/2010 8:40 AM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi T41, as well Yersaid, seems you booked the missing PO from other licence. Project uses 2049 PO, engineering has 1700 PO (93 available): no possible download all program with that PO number (1700), the ONLY possibility is you used a different ES to download it (the otherpossibility could be using download "To Test CPU" but is very hard to use it on the running plant) P.S.: when AS RT PO max nr. reached the system will notice you need expand your license and permit you to download program anyway Can you post a screenshot about how many PO booked into multiproject, please? (follow the link cumulusgave above) If booked license number is greater than license nr on ES means you go them from other part hope can help regards |
Follow us on