2/22/2010 9:55 AM | |
Posts: 2930 Rating:
|
Hi, in short form: 1. You have to config the Master with the Wizard in MW 2. Each PLC in the network requires a different Station-Adress (Systemblock) 3. The Data you can excanche are located in V-Memory 4. up to 126 units can be connected to a PPI network 5. You can also connect a PC to the network More information you can find: 1. S7-200 System manual Chapter 7 2. S7-200 Programming Tips on the second CD of MW 3. FAQ's : http://support.automation.siemens.com/WW/view/de/22634774 http://support.automation.siemens.com/WW/view/de/22635121 http://support.automation.siemens.com/WW/view/de/12970349 The best is to test it by your selve. It is not an complicated task. |
Follow us on