2/25/2010 4:44 PM | |
Joined: 3/14/2008 Last visit: 9/4/2025 Posts: 2216 Rating:
|
Hello, The last couple of days I'm collection information for the selection of a new cpu which runs under pcs7.1. I can't figure out which CPU we need to choose.. It is also important for feature purposes because now I only do single client OS with one AS. For the feature, there will be two OS stations with redundant server and possibly another CPU. Think of a time span for 1 year or so... I came up with two selections... The 417 I think has too much overhead, since the total I/O is 1000, with six ET200M + a few s7300 CPU's and a total of 800 I/O for exchanging data to/from drives. Let's say that we need three more ET200m fully equipped in the future... Further, the actual data size of the program is as follows: - System data memory = 22534 bytes - User program memory->Load memory = 1284342 bytes - User program memory->Work memory = 1023204 bytes I'm halfway with the project. It is difficult to determine. So far, I didn;t find any good guidelines when selection a cpu... Can somebody point me in the right direction? Thank you |
If I could help you, you can use the RATE button. Thank you. |
|
2/25/2010 6:19 PM | |
Joined: 11/15/2009 Last visit: 11/5/2024 Posts: 385 Rating:
|
Hello Oreca, To reach a decision can help the tool "ProTime". http://www.automation.siemens.com/w2/automation-technology-protime-3749.htm Regards |
3/2/2010 11:27 AM | |
Joined: 3/14/2008 Last visit: 9/4/2025 Posts: 2216 Rating:
|
Hello JOTST, Thank you for the suggestion. There is a tab where I can calculate some stuff.... |
Last edited by: Oreca at: 3/2/2010 11:29 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on