3/6/2010 12:17 AM | |
Posts: 1 Rating:
|
Hi, I am using Step 7-MicroWIN 32 v 3.2.0.105. When trying to add PC/PPI cable in "Set PG/PC Interface" module, a problem occurs with file S7EPATDX.cpl. First time this problem occured during instalation of Micro/WIN 3.2 and is still present. The same failure appears when using Step 7-MicroWIN 32 v4.0 - there are some problems with comm200I8host.exe and mfc42.dll. More information avalible in e716_appcompat.txt file, which was generated by the aplication. System: Windows XP Professional SP3 It is a bit urgent, so looking forward for help. Regards Hubert Attachmente716_appcompat.pdf (213 Downloads) |
3/8/2010 7:54 AM | |
Joined: 9/28/2005 Last visit: 7/24/2025 Posts: 2957 Rating:
|
Hello, First of all check Step-7 Micro/Win comaptibility list here. Then you might want to update to SP7. You will find it here. After all this you system must be compatible and check if error still exists. Please report it here. |
Best regards, |
|
Follow us on