3/10/2010 3:30 AM | |
Posts: 6 Rating:
|
Dear all, My PLC is "S7-200" use "STEP 7- Micro/WIN" to do the PLC program. CPU is EW 277 profibus-DP My HMI is "TP177Micro Touch Panel" use "WinCC flexible Advance 2008" to do the graphic design. And I also have TD200 to be connected. Now I want to integrate S7-200 with TP177Micro Touch panel. I cannot use WinCC flexible 2008 "Integrate in STEP 7" option to do the integration, because the integrate function does not support S7-200. And from this Q&Ahttp://support.automation.siemens.com/WW/view/en/38797081, look at bottom of the page. It tells that "You cannot integrate Micro Panels, e.g. a TP177micro, into STEP 7." Can I use profibus to integrate S7-200 and TP177Micro? Anyone can help me? Zoe
|
Last edited by: ZOEZHAO at: 3/10/2010 3:39 AMLast edited by: ZOEZHAO at: 3/10/2010 3:33 AM |
|
Follow us on