8/15/2010 4:42 PM | |
Posts: 89 Rating:
|
Dear All I am working in a system where I have to show one Stand alone Existing System and four other New Systems. My New Systems are working fine in WinCC , But for the Existing Stand Alone System I took the WinCC Backup , copied the Tags with Configuration tool and inserted the Tags in my New Project. I got Problem with these Tags in the Runtime; as I activate the Wincc , It shows the correct data in the First Activation. But when I change the Areas in the Runtime and come back to the same Area , it shows some problem in that. Attached file contain the snaps of the problem. AttachmentSNAPS.zip (78 Downloads) |
8/16/2010 7:33 PM | |
Posts: 89 Rating:
|
I have checked all the Tags and there is no any problem I am getting the Problem with 75 % Tags Don't know the reason |
Follow us on