8/23/2010 2:31 PM | |
Posts: 159 Rating:
|
Hello! I have a PCS 7 v7.0 Sp3 with ES, one OSClient and one OSServer setup. I have some problems with the SFB35 (Alarm_8p) block in my CFC. I have configured the block as opposed in the documentation (had not this problem when my system were running as singlestation). After compile\download, when the "SIG_1" on the Alarm_8P i true, the alarm shows in WinCC. So far so good But my problem is that the Message text is missing in WinCC! Could this be because of my "Standard server" settings in the client? (see submitted picture) I must admit that I dont have full understanding of the standard settings... AttachmentMessage text.zip (158 Downloads) |
9/10/2010 2:55 PM | |
Posts: 159 Rating:
|
Runis, Thank you very much for your reply. Tride what you suggested and it worked. |
Follow us on