4/13/2011 9:23 AM | |
Posts: 7 Rating:
|
hi guys
I have cpu 313c-2dp and MM440 , I downloaded an example from http://support.automation.siemens.co...ew/en/22078757 I tryed these but it doesn 't work , I only set HW config to my property set profibus addres to 3 and copy the block of exampel to my program , should I chenge the fc14 or ob1 's program? I set P700 and P1000 to 6 I just wanna play and test and know how it works? there is F0070 on my MM440 what should i do? please help me thanks before I attached my program AttachmentFc14_dpe.zip (177 Downloads) |
4/14/2011 3:58 PM | |
Posts: 739 Rating:
|
pls. have a look into this FAQs: http://support.automation.siemens.com/WW/view/en/22329309 http://support.automation.siemens.com/WW/view/en/25339501 http://support.automation.siemens.com/WW/view/en/12324244 |
4/16/2011 12:16 PM | |
Posts: 7 Rating:
|
eny other help,reply ???? |
6/1/2011 8:34 PM | |
Posts: 63 Rating:
|
Hello, From Drive side following parameter reuired to set. Cmd source P700-6 Set point source P1000-6 Above parameter index will be 6 in corresponding to CDS selection. Profibus address value Find the attachment. Regards Pranab |
Follow us on