6/25/2011 12:58 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, In simple V/F mode, motor speed is varied by keeping V/F ratio constant. What torque constant is meant by, whenever there is requirement of constant torque during the complete range i.e. say from 1 to 50 Hz, drive will supply & at the same time motor will draw rated current, say in your case 6.6 Amp. As long as drive part is considered, there will not be any problem. But the motor at low RPM say at 1 Hz, should be capable to deliver the torque & heat dissipation must be OK. Otherwise because of overheating & longer time duration of operation, motor may fail. |
Follow us on