12/14/2006 9:07 PM | |
Posts: 1 Rating:
|
Problem: A S7-414FH system.(maybe this information is not important) I used step 7 and went online to talk to the PLC from the computer. I tried to monitor some logic or DB block (click the "glass" icon for monitor variables online). It seems just work several seconds then no response and popup an error message "connection disrupted".Click help button show "Help on message 33:16654". Due to this problem I can't debug the program. Now the situation is we have full redundant remote station profibus address=3,4,5,6,7. Additional profibus address=1,8 represent the laser weighting systems for two units. They are connected in just one profibus system,that is, no redundant.These two profibus 1&8 are integrated in the whole system through HWconfiguration. But they are not really connected into the system now. Is it the reason to cause the problem? As from the help, one suggestion is "check any remote connections". If that's the reason, do I need to delete them from the HWconfiguration? How about the corresponding program? Thank you! Any suggestion can be forward to bwu@enersul.com Attachmentproblem_online_monitor.pdf (680 Downloads) |
12/19/2006 5:12 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello, |
Follow us on