(0)| 9/9/2011 4:01 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, S7opcsrtx concerning PROFINET IO RT-Protocol (LLDP). Check if the enabled Ethernet board for the communicatuon have the protocols: Profinet IO RT-Protocol , Profinet IO RT-Protocol(LLDP), Simatic Industrial Ethernet (ISO), TCP/IP. If you didn't install yet Service Packs 1 for STEP 7 V11 and Updates for STEP 7 V11 SP1 and WinCC V11 SP1 - make it. Then if this doesn't help - reinstall of TIA11. Hope didn't go in wrong direction. Best regards, Hristo Mihalev |
Follow us on