10/24/2011 9:31 PM | |
Posts: 2 Rating:
|
I am commissioning MM430. For a fast stop I wish to use DC braking. However on BOP screen DC-braking is displayed, and really it is not present. Differences between time with simple a stop and with a stop with DC-braking are not present. Parametres P1230, P1232, P1233, P1234 do not change to a situation. My file .dnl is attachment. Attachment110803_MICROMASTER 430.ZIP (175 Downloads) |
10/26/2011 12:36 PM | |
Posts: 739 Rating:
|
pls tray p1240 = 0 (disables Vdc-max controler) |
Follow us on