12/22/2011 11:54 AM | |
Posts: 11 Rating:
|
find this attachment......4 u
Attachmentmicro master 440 connection.pdf (364 Downloads) |
This contribution was helpful to
1 thankful Users |
12/22/2011 11:59 AM | |
Posts: 139 Rating:
|
Dear all, Thanks for your prompt reply. will try out again. |
12/22/2011 12:27 PM | |
Posts: 139 Rating:
|
|
12/22/2011 1:51 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi, Its difficult to say whether the AOP or the Drive is at fault here. Clearly, the AOP could be defective, or the power supply for the AOP electronics, or the connector etc. Anyway, here are the settings for the switches, both the ones on the interface board and the ones behind the interface board. Regards, Graeme
AttachmentSwitch_Settings.pdf (332 Downloads) |
This contribution was helpful to
1 thankful Users |
12/25/2011 10:42 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
I Agree with Graeme that Mostly AOP is looking damaged in this case, but also can be Power Supply of Drive also so please connect AOP directly to the drive (NO PROFIBUS MODULE) as suggested by Graeme And regarding dip switches, I think C.ktis talking about dip switches given on the back side of AOP
there is NO information available that what is the use of this switch....Some one from forum said that its for internal repair use... You may be knowing about these swithcesGraeme Regards Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on