12/30/2011 5:19 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Question :- How Many motors you are going to connect with a single drive? If it is One Drive-One Motor System then Encoder Module will work for you. For Multi motor application, you have to connect Encoder to any one motor Regarding starter connection, there are several Options Best one is you have to purchase Drive-PC Connection Kit (6SE6400-1PC00-0AA0) Another is, use RS485-232 Converter and connect using RS485 terminals of Drive (Terminal 29 & 30) Also have a look at (How do I set up my MM4 with Starter or DriveMonitor?) for More help Regards Devesh Vithani |
Last edited by: Vithani at: 12/30/2011 5:23 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
12/30/2011 7:10 PM | |
Posts: 2 Rating:
|
Yes it is just one motor, so thats good news about the encoder module. I might use Profibus for my starter connection. |
Follow us on