1/17/2012 3:00 PM | |
Posts: 376 Rating:
|
Hello m.shakshoki1, my question is: Is your problem already solved? If not, I still have the following questions. 1. Which equipment (Hardware, Devices) would you like to physically connect with this adapter? 2. Which functions would you like to realize with this HMI adapter V5.1? Unfortunately, I do not have any driver at the disposal, but this entry in the manual is right. "The operator interface device must have a suitable driver in order to communicate with an S7/M7/C7 system via the HMI adapter. This driver is part of the operator interface device." Best Regards Azteke0110 |
1/31/2012 2:37 PM | |
Posts: 376 Rating:
|
Hello m.shakshoki1, Notes! 1. Product Definition for the HMI Adapter with the order number 6ES7 972-0CA1X-0XA0. The HMI adapter (HMI = Human Machine Interface) connects an operator interface device (OI) without a multipoint/DP interface, to the multipoint/DP interface of an S7/M7/C7 system. The operator interface device for example, OP (Operator Panel) must have an RS232 interface. 5.2 Software The operator interface device must have a suitable driver in order to communicate with an S7/M7/C7 system via the HMI adapter. This driver is part of the operator interface device. The Quick Reference Guide for the HMI Adapter finds you here: http://support.automation.siemens.com/WW/view/en/8774263 Please take into account! But if you wants to realize a communication between a PG/PC with STEP 7 software and a S7-300 PLC, then you need a PC Adapter. For example PC Adapter V5.2 with the order number 6ES7 972-0CA23-0XA0 The Quick Reference Guide for the PC Adapter finds you here: http://support.automation.siemens.com/WW/view/en/14053309 The PC adapter V5.x connects a PC to the MPI/DP interface (Multipoint Interface) via the serial COM port of an S7/M7/C7 system.This does not require a PC slot, that is, the adapter is also suitable for use in non-expandable PCs such as notebooks. If your PC has a USB interface then you can use the PC Adapter USB. Information about this hardware find you here: http://support.automation.siemens.com/WW/view/en/16983464 Best regards Azteke0110 |
Follow us on