3/15/2012 8:58 AM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello, I think you can use the interface parameter about the signal persecution with the interconnection, which do you can use in each plan. Call the RAMP_P in a FB or FC and go with the parameterized variables to the interconnection of the plane. The following FAQ has not a description of a RAMP_P but shows an example which do you use the interconnection. http://support.automation.siemens.com/WW/view/de/22904741 With best regards |
Follow us on