9/1/2012 5:17 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Hello , There is no magic shortcut to accomplish the task.You should understand the whole logic and then write them in SCL. For basic programming , it is not very difficult and somehow more convenient.I also recommend you visiting the following clustered threads for a quick start: HD_SCL Starting Point Best regards Hamid Hosseini |
9/1/2012 7:22 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Hello,
The negative answer is always unpleasent we should consider technical issues on our decisions.
SCL is a high level language and implementing an existing FBD project in SCL is time consuming .It would be a trade off between necessity and time you can spend. Also check this previously discussed similar issue here: LAD to SCL
Best regards, Hamid Hosseini |
Follow us on