4/30/2007 12:29 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello, regarding to your inquiry we would like to inform you. The error message in refer to your STEP 7 software could have the following reasons: - STEP 7 is not compatible with your installed operating system. - STEP 7 is not compatible with one of the installed optional software (S7-GRAPH, CFC, ...). - One of installed optional software is not compatible with your operating system. - Not enough free space of your hard disk. - The adjustments of the virtual work memory are to little. Please see the informations of the following FAQ, which do you will find by the customer support in the internet: http://support.automation.siemens.com/WW/view/de/8250891 http://support.automation.siemens.com/WW/view/de/22645302 http://support.automation.siemens.com/WW/view/de/24059046 |
Follow us on