11/12/2012 10:40 AM | |
Posts: 5 Rating:
|
Hi Guys Good day and hope you doing fine I've analog output card(6ES7332-5HD01-0AB0) configured with 0-10 v theory and actually I'm trying to operate an motor with 50% form its velocity and tried to join the actuator to the analog output card pins for times and with differs ways pin 5and6 ,pin 4and5 but unfortunately there is no output voltage can some one help me plz is there and wrong with program?(See attached) or there is something in wiring ? Best regars
AttachmentAnalog_i.zip (237 Downloads) |
11/12/2012 10:48 AM | |
Posts: 1064 Rating:
|
in network the move statement is move mw214 to qpw304 and i think it should be md212 |
11/12/2012 10:56 AM | |
Posts: 5 Rating:
|
Thanks for your attention but thats represent the upper word and it should take the value,other supports if its possible. regards
|
11/12/2012 11:03 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Program sends 13824 to output (in simulation), so that should be o.k. You have to wire like attached pdf. bridge 3&4 and bridge 5&6 conect load at 3 and 6 (M ana) Regards, Marcjan Attachmentanalog_output.pdf (260 Downloads) |
Problem solved? |
|
11/12/2012 11:06 AM | |
Posts: 1064 Rating:
|
actually it's the lower word in siemens not the upper |
11/12/2012 12:40 PM | |
Posts: 5 Rating:
|
you alright its the lower i got mistake |
Follow us on