6/14/2013 4:35 PM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello, firstly check the fault history, there the lasseven and the actualfaults are stored. Use the DriveMonitor tool With the DriveMonitor also a trace with trigering on fault or on a certain drive condition (status word 1)and a preetriger can be done. I would trace the the control word 1, in order to exclude, that the prpblem hasn't the control as origin. As described by you, it seems, that the problem comes from outside. Please refer also to the masterdrives CUVC compendium, esp. the function diagrams. |
With best regards, |
|
6/22/2013 3:13 PM | |
Posts: 27 Rating:
|
Hi, do you get any fault value while it is getting tripped.? or drive is just getting off.? Regards, |
Follow us on