(0)| 7/15/2013 11:16 AM | |
|
Posts: 9 Rating:
|
Hi all; I am trying to model G120+induction machine set at matlab simulink.I am doing this in order to see big inertia affect on dynamics of the machine (big inertia mismatch).Our G120 are working under SLVCtherefore P1300=20 and P1501=0 are already chosen.But according to function diagram G120 also configure P1715 P1717 P1764 P1767 but they are not seen at parameter list.What should I do? Thank you very much for your consideration.. At attached file you can see functional diagram of G120 SLVC Regards Yaylaci AttachmentG120_Control Units2.pdf (534 Downloads) |
| 7/15/2013 3:55 PM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Yes, as said by sparten, these will need access level 4 But better parameterisation of SLVC in G120, have a look at following FAQ MICROMASTER 440 (MM4), SINAMICS G120 (CU2x0x): How can I use Sensorless Vector Control (SLVC) on the MM440 or SINAMICS G120 (CU2x0x)? Regards, Devesh Vithani |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
|
|
Follow us on