Type: slip ring motor
Power: 250 Kw
Applied voltage:380 V
Application: Fan
R.P.M:1450
7/30/2013 11:38 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, What you want to control in slip ring induction motor? Basically slip ring induction motors are used for high starting torque & fixed speedapplication e.g. cranes, compressors etc. Its rotor is wound rotor & depending upon torque requirement external resisitors are added in rotor circuit during starting. So there is no any functional requirementof drive. If you want to very the speed,with proper engineering,motor needs to be replaced with adequate capacity motor & drive. |
Follow us on