8/15/2013 10:11 AM | |
Posts: 3609 Rating:
|
Import of a Technical Question of the User bullet3255
|
8/28/2013 7:02 AM | |
Posts: 18 Rating:
|
leave it the old problem . we will discuss it later. this is a new problem which i am facing. i have the license in the pc . due to the problem of computer , i want to transfer that in to pen drive . i attached the 8gb pendrive. the error is appearing during transfer . kindly find the attachment. 1 ) is there any separate pendrive is there to transfer the keys? 2) what is the procedure to transfer the license key.? i will explain u that what i was exactly . i opened automation license manager , then i select the particular license right click it , then select transfer , then i select the pendrive as a my destination. still the problem is there.
Attachmentlicense1.pdf (459 Downloads) |
8/28/2013 11:19 AM | |
Posts: 3037 Rating:
|
Hello, Is the licence ok? You can check this with right mouse click on the licence. Have a look in the link. See chapter 5. http://support.automation.siemens.com/WW/view/en/27005215 Tweety |
Follow us on