10/14/2013 5:08 PM | |
Posts: 2 Rating:
|
Hi, I am having trouble getting online with a Masterdrives MC via RS232. When I connect the cable and try to set up an online connection (File menu\Set up an USS ONLINE connection) Drive Monitor reports back with invalid COM-port or port in use. My cable is made as follows: PC pin 2 to X103 pin 7 PC pin 3 to X103 pin 2 PC pin 5 to X103 pins 1,5,9 Is this cable correct? I set the following parameters: P701=6 P702=127 P703=2 P053=6 AttachmentDRV-MasterDrives-DriveMonitor_docs.pdf (897 Downloads) |
Last edited by: sgop013 at: 10/14/2013 6:13 PMI found the correct cable according to the attached tutorial and followed the instructions within. The same error occurs when I try to go online. Last edited by: sgop013 at: 10/14/2013 5:34 PM |
|
10/15/2013 5:38 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating:
|
Hello, that could be a problem of your laptop. Is it possbile to check it with a laptop from a collegue? Zako |
Follow us on